Technical FAQs

Ask a Question

What are the assignment options for the digital outputs of Lexium 32 M ?

Lexium 32 M has three digital outputs which can be used to indicate various drive status bits.
Attached you will find a small PDF file which provides data regarding these outputs.

The first page shows the functional status flow of the No Fault and Active outputs
The second page shows the factory default assignment of the outputs based on the selected default operating mode.
The third page shows all of the available assignments that the outputs can be configured as.
Was this helpful?
What can we do to improve the information ?