Technical FAQs

Ask a Question

What is the largest PCMCIA memory card I can get for the TSXP57303M Premium controller?

Issue:
What is the largest PCMCIA memory card I can get for the TSXP57303M Premium controller?

Product Line:
TSXP57303M, Premium, PCMCIA memory card

Environment:


Cause:


Resolution:
The Premium TSXP57303M will support 384K words and that's only available in the SRAM type memory cards. For the EPROM, it will max out at 128K words.  Below are the part numbers of the memory card:

TSXMRPC002M - SRAM memory card
TSXMRPP384K - Flash EPROM memory card
Was this helpful?
What can we do to improve the information ?