Technical FAQs

Ask a Question

Why am I getting an error message: "Can not find BMPxx" when trying to press a button/switch on the Magelis after downloading?

Issue:
Why am I getting an error message: "Can not find BMPxx" when trying to press a button/switch on the Magelis after downloading?

Product Line:
Vijeo Designer, Magelis

Environment:


Cause:


Resolution:
That error usually means that one of the bitmap (BMP) files were not downloaded to the magelis successfully.  Recommended to try the following to resolve the issue:

1 - Try to load the project again from the USB stick
2 - Use a different USB stick to load but first format the USB stick as FAT32.
3 - Maybe this issue with the project.  Duplicate the target and then try redownloading as filesystem to the stick again or directly to the target.
Was this helpful?
What can we do to improve the information ?