Technical FAQs

Ask a Question

How to install the DTM files for the BMXNOC0401?

Title
DTM files for the BMXNOC0401
 
Issue
DTM files for the BMXNOC0401
 
Product Line
M340 BMXNOC0401
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
 To install the DTM file for the BMXNOC0401, run the installation executable located in the LOKI DTM folder that is on the Unity 10 install CD.
Was this helpful?
What can we do to improve the information ?