Technical FAQs

Ask a Question

Does the Quantum CPU Ethernet port have a Logout Button on it's webpage?

Title
Quantum CPU Ethernet port Logout capability
 
Issue
Quantum CPU Ethernet port Logout capability
 
Product Line
Quantum
 
Environment
Quantum Ethernet pages
 
Cause
N/A
 
Resolution
 The Quantum CPU has a Logout Button in the webpage with firmware 5.0 or higher. This firmware version or higher provided the functionality to log out users from PLC programming via the web page. To access this functionality, go to the Diagnostics page then select Rack Viewer. Next, right-click on the controller image and select Controller Status. Clicking on the Log Out button will creat a new pop up confirming the users request.
Was this helpful?
What can we do to improve the information ?