Technical FAQs

Ask a Question

Why am I getting error 6003 Hex on a Concept MBP_MSTR function block but still receiving data on my M1E?

The M1E has an on-board set of diagnostics for the MBP_MSTRs.  In this case, it is indicating that the connection was closed prematurely by the slave device. The exact definition of the error is "Early Fin received". The slave device aborted the connection instead of closing it or the remote node is running out of resources..
 
Was this helpful?
What can we do to improve the information ?