Technical FAQs

Ask a Question

What is the difference between a M580 Main IP Address and IP Address A (&B) ?

Title
M580 Main IP Address and IP Address A (&B)
 
Issue
M580 Main IP Address and IP Address A (&B)
 
Product Line
M580 PAC
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
 For the M580, the Main IP Address is the address of the CPU and the IP Address A (& B) is the IP address of the EIO scanner service (IP address B – used for Hot Standby).
NOTE: If you change IP address A, the system may recalculate all IP addresses (including those of the drops) to keep all devices in the same subnetwork.
Was this helpful?
What can we do to improve the information ?