Technical FAQs

Ask a Question

What is the difference between a Rev 1 and Rev 2 TSXCUSBMBP ?

Title
TSXCUSBMBP Rev1 versus Rev2
 
Issue
TSXCUSBMBP Rev1 versus Rev2
 
Product Line
TSXCUSBMBP
 
Environment
Modbus Plus
 
Cause
N/A
 
Resolution
 The difference between a Rev 1 and Rev 2 TSXCUSBMBP converter is that the Rev 2 TSXCUSBMBP is upgradeable.
But the TSXCUSBMBP REV1 adapter can not be upgraded.
Was this helpful?
What can we do to improve the information ?