Technical FAQs

Ask a Question

Does the M580 support Hotstandby Remote IO (S908)?

Title
M580 support for Hotstandby Remote IO (S908)
 
Issue
M580 support for Hotstandby Remote IO (S908)
 
Product Line
M580 PAC
 
Environment
Unity pro
 
Cause
N/A
 
Resolution
 The M580 PAC is planning to support HotStandby Remote IO (S908) by the third Quarter of 2016.
Was this helpful?
What can we do to improve the information ?