Technical FAQs

Ask a Question

How many READ_VAR and WRITE_VAR can be active at the same time in a BMXP342020 controller?

Up to 16 READ_VAR and WRITE_VAR can be active at the same time.
Logic is require to sequence up to 16 READ_VAR and WRITE_VAR function blocks at the time.
Was this helpful?
What can we do to improve the information ?