Technical FAQs

Ask a Question

What Unit ID is needed for a Tesys T IO Scanner connection?

Title
Tesys T Unit ID
 
Issue
Unit ID for IO Scanner connection to Tesys T
 
Product Line
Tesys T
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
 When setting up a IO Scanner connection to a Tesys T via ModbusTCP, set the Unit ID value to 254.
Was this helpful?
What can we do to improve the information ?