Technical FAQs

Ask a Question

How to change the IP Address on a 170ENT11001?

 Title
Advanytys 170ENT11001 IP Address Change
 
Issue
Need procedure to change the IP Address on a 170ENT11001.

Product Line
170ENT11001
 
Environment
Default Wepbpages
 
Cause
N/A
 
Resolution

Below is the procedure for changing the IP Address on a 170ENT11001.

Using either option will store the IP address into the 170ENT11001.

1. You can change the IP address via the webpages. (page 49).

2. You can change the IP using bootplt ( If BootP is not disabled. see note below.)

3. You can write to the configuration registers with ModbusTCP. (Configuration Save/Get Current IP Address via registers on page 66).

 

Using either option will store the IP address into the 170ENT11001. For more information please reference the Obtaining an IP Address section on pages 33-34 of the User manual.

Note: If the Disable BOOTP/DHCP Request, Use the Stored IP Parameters (see page 49) is selected on the Current IP Configuration Web page and there is a static IP address stored in the adapter, no request will be sent to a BOOTP/DHCP server.

Was this helpful?
What can we do to improve the information ?