Technical FAQs

Ask a Question

What PLC processors can be used with the M340 Modbus Plus Proxy (TCSEGDB23F24FA) ?

Title
M340 Modbus Plus Proxy (TCSEGDB23F24FA) supported PLCs
 
Issue
Supported PLCs for the M340 Modbus Plus Proxy (TCSEGDB23F24FA)
 
Product Line
TCSEGDB23F24FA, M340, M580, Unity Momentum
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
The M340 Modbus Plus Proxy (TCSEGDB23F24FA) can only connect and communicate to a M340, M580 or a Unity Momentum. Other devices will not work.
Was this helpful?
What can we do to improve the information ?