Technical FAQs

Ask a Question

Can one have 2 sets of LPCTs for the SEPAM relays?

Is it possible to have more then one set of LPCTs?

Product Line
SEPAM 20, 40, 50, 60, & 80

Ordering relay parts

The design of the SEPAM relay is to only accept one set of LPCTs for all SEPAM models.

The SEPAM can not accept two sets of LPCTs. The other set of cts must be a standard protection cts with a 5 or 1 amp secondary that are wired into the CCA634 or CCA630 on the SEPAM.
This option is only available on the differential SEPAM 80 series relays. 
Was this helpful?
What can we do to improve the information ?