Technical FAQs

Ask a Question

Preventa XY2C - Dimensions of the XY2CZ712 end-spring

Find attached dimensions of the XY2CZ712 end spring. It is suitable for XY2CED E.stop rope pull switch installation, in quantity of 2.
Attachment shows image of this XY2C accessory and gives material.
Was this helpful?
What can we do to improve the information ?