Technical FAQs

Ask a Question

Osisense XC_What is the ZCKY45 lever? Can we order it in 2015?

1) ZCKY45 lever is the variable length thermoplastic roller lever used in the obsolete XCKP XCKT plastic limit switches, black casing. Attached product picture.
2) In 2015, it is still available to order for spare parts of this obsolete range. It is in stock in our international distribution centre in France.
3) In the current range of XCKP XCKT blue limit switches, plastic case; equivalent lever for this blue range is the ZCY45 lever. Please note that the ZCY45 lever is positive for safety applications, not the old ZCKY45 one.
Was this helpful?
What can we do to improve the information ?