Technical FAQs

Ask a Question

What is a 1401831Q module and who supports it?

Issue: Support

Product Line: Quantum

Environment: None

Cause: Procurement and Support

Resolution: The 1401831Q is a single channel resolver interface module for the Quantum platform and is made by AMCI - Advanced Micro Controls Inc.,  a CAPP partner.

For procurement and support questions on this module, please contact

AMCI Corporate Headquarters
20 Gear Drive
Plymouth Industrial Park
Terryville, CT 06786

Tel: 860-585-1254
Fax: 860-584-1973

Tech Support:

Was this helpful?
What can we do to improve the information ?