Technical FAQs

Ask a Question

What is the replacement part number for Lexium 05 drive bearing part number LXM05BD10M2?

Issue: Replacement


Product Line: Lexium 05B


Environment: None


Cause: Obsolescence


Resolution:

The corresponding part number to replace a LXM05BD10M2 will be a LXM32MU90M2 in terms of current rating. Lexium 05B is a Profibus drive and hence the option card VW3A3607 needs to be ordered as well. Importing the GSD file for the Lexium 32 in the PLC program and some configuration changes at the drive are to be expected. Profibus command structure between Lexium 05B and Lexium 32 is very similar and so it should not call for significant programming changes. Some programming changes are to be expected.
Was this helpful?
What can we do to improve the information ?