Technical FAQs

Ask a Question

Osisense XM_XMPC12C2941C701 specifications and how to order in 2015

1) The XMPC12C2941C701 power switch is the "standard" XMPC12C2941 (available under logistic ref. XMPC12C2941AB in 2015, requesting to provide the fluid entries A, B, C, D definition), supplied with C701 specification.

2) C701 specifications meaning
  • 1/2 gas fluid connection drilling in A (see attached file for fluid entries designation)
  • 1/4 gas fluid connection drilling in C
  • B and D closed
  • Pressure adjustments : factory settings 2,0-3,5bar.
3) How to order the XMPC12C2941C701 reference in 2015 : it has to be ordered under the following logistic reference XMPC12C2941C701AB (internal Schneider rule); nothing to define at order. Logistic situation : available, manufactured at order reception.
Was this helpful?
What can we do to improve the information ?