Technical FAQs

Ask a Question

What wire gage can be used on the M340 discrete 16 point modules?

Attached is the specifications for the wiring gage for the 8 and 16 point discrete modules.
Was this helpful?
What can we do to improve the information ?