Technical FAQs

Ask a Question

What is the maximum wire gage an STBXTS1110 terminal can accept?

Issue:
What is the maximum wire gauge that a STBXTS1110 terminal can accept?

Product Line:
Advantys STB

Resolution:
The STBXTS1110 and STBXTS2100 terminals accept wire sizes from 24 to 16 awg.
Was this helpful?
What can we do to improve the information ?