Technical FAQs

Ask a Question

Osisense XS_XS518B1DAP5TF datasheet

Please find attached the datasheet of the XS518B1DAP5TF adapted sensor, not shown in the Osisense XS catalogue.
The TF suffix meaning is extended low temperature range to -40°C in operation. P5 means it is supplied with a PUR cable of 5m length.

The sales of such product are open for all customers in 2015. It is not in stock (produced at order reception).
Was this helpful?
What can we do to improve the information ?