Technical FAQs

Ask a Question

Osisense XS_XS1N30PA349SBTF datasheet

Please find attached the datasheet of the XS1N30PA349SBTF adapted sensor, not shown in the Osisense XS catalogue.
The TF suffix meaning is extended low temperature range to -40°C in operation. SB means it is supplied with a pigtail M12 4pins connector + 0,1m cable length.
The sales of such product are open for all customers in 2015. It is not in stock (produced at order reception).
Was this helpful?
What can we do to improve the information ?