Technical FAQs

Ask a Question

Osisense XS_XSAV12373TF datasheet

Please find attached the datasheet of the XSAV12373TF adapted sensor, not shown in the Osisense XS catalogue. The TF suffix meaning is extended low temperature range to -40°C in operation.
The sales of such product are open for all customers in 2015. It is in stock.
Was this helpful?
What can we do to improve the information ?