Technical FAQs

Ask a Question

Do we offer a Modbus RTU to TCP (serial to ethernet) gateway?

Issue:
Do we offer a Modbus RTU to TCP/IP  gateway?

Product Line:
Modbus RTU, gateway, serial to ethernet

Environment:


Cause:


Resolution:
Yes, the part number for the serial to ethernet gateway is TSXETG100
Was this helpful?
What can we do to improve the information ?