Technical FAQs

Ask a Question

What is the speed and torque rating of Lexium Integrated Drive type ILE2x661 ?

The Lexium Integrated drive type ILE2x661 without gearbox has the following ratings.

At 24 vdc supply the motor has a nominal torque rating of .26Nm and a nominal speed rating of 4800rpm

At 36 vdc supply the motor has a nominal torque rating of .26Nm and a nominal speed rating of 6000rpm

See attached file for the complete speed/torque information


Rev 9-18-17
Was this helpful?
What can we do to improve the information ?