Technical FAQs

Ask a Question

How montior a specific LAN with ConnexView on a PC that has more than 1 NIC.

Goals and Symptoms
How to montior a specific LAN with ConnexView on a PC that has more than 1 NIC.

Facts and Change
ConnexView

Causes and Fixes
When you first click on Tools\Discover Network, a default 'Network Discovery Parameters' window will appear.  It will show
all of the defined IP addresses for all of the NIC's on the PC.
User-added image


In the screen capture shown below, the wireless NIC is set at IPO address 10.169.24.0 (corporate network) and the
wired NIC is set IP addresses 192.168.x.x (PLC network)
User-added image.


If you click on 'OK' in the 'Network Discovery Parameters' window and apply the results when the discovery i s completed,
the 'Netwok Devices'will show results for both LANs.
User-added image


If you just want to monitor only one of th eLANs (i.e., the wired NIC), use the following steps:
  • Open the 'Network Discovery Parameters' window.
  • Delete the listed subnet IP address for the LAN that you do not want to monitor.
  • Specify only the subnet IP address for the LAN that you want to monitor.
  • Click on OK.
User-added image
 
  • Click on Apply after the discovery completes..
User-added image


User-added image
Was this helpful?
What can we do to improve the information ?