Technical FAQs

Ask a Question

Osisense XM_XMLCS35B2S12SB5 datasheet

The XMLCS35B2S12SB5 is an adapted pressure switch based on the standard XMLCS35B2S12 30bar overpressure, with some pressure adjustement made in production plant. Please find attached the XMLCS35B2S12SB5 datasheet, origin EAC or Sensors Adaptation Centre in France, giving the adjusted pressure values (PH=0,35 PB=0,29). Please note that the XMLCS35B2S12SB5 reference sales are reserved to the german OEM who asked for.
Was this helpful?
What can we do to improve the information ?