Technical FAQs

Ask a Question

Regarding the Magelis XBTGT/HMIGTO with embedded Ethernet, when using the XBTZGUMP USB/Modbus Plus gateway. Is it possible to simultaneously use the Ethernet port for Webgate and iPad/iPhone?

Issue:
Regarding the Magelis XBTGT/HMIGTO with embedded Ethernet, when using the XBTZGUMP USB/Modbus Plus gateway. Is it possible to simultaneously use the Ethernet port for Webgate and iPad/iPhone?

Product Line:
XBTGT, HMIGTO, XBTZGUMP

Environment:


Cause:


Resolution:
 There are no conflicts between the XBTZGUMP and the embedded ethernet port on the XBTGT/HMIGTO target.  It does not matter if you use the ethernet port for communications to a controller or Web Gate, you should be able to simultaneously have communications to both the XBTZGUMP and ethernet port.
Was this helpful?
What can we do to improve the information ?