Technical FAQs

Ask a Question

What are the error codes for the Momentum Unity processors using the XXMIT?

X/XMIT ComSys Error Codes
 
Value Error Description
16#00 Correct exchange
16#01 Exchange stop on timeout
NOTE: OK value returned when a Modicon M340 CPU sends a MODBUS BROADCAST request
16#02 Exchange stop on user request (CANCEL)
16#03 Incorrect address format
16#04 Incorrect destination address
16#05 Incorrect management parameter format
16#06 Incorrect specific parameters
16#07 Problem in sending to the destination
16#08 Reserved
16#09 Insufficient receive buffer size
16#0A Insufficient send buffer size
16#0B No processor system resources
16#0C Incorrect exchange number
16#0D No telegram received
16#0E Incorrect length
16#0F Telegram service not configured
16#10 Network module missing
16#11 Request missing
16#12 Application server already active
16#13 UNI-TE V2 transaction number incorrect
16#FF Message refused
Was this helpful?
What can we do to improve the information ?