Technical FAQs

Ask a Question

EnerSure BCPM Installation Guide

User looking to access BCPM webpage and possibly perform firmware upgrade.

Product Line
EnerSure BCPM from TrendPoint

Installation Guide

Installation procedure, communication trouble shooting.

Refer to attachment to download the installation guide.  It includes topics like hardware, communication, device setup, using web interface, firmware upgrade and more.

Page 24: In order to use the web interface, open a browser and enter IP address of the device.  Use 'adminpass' as the password to login.
Page 27: Firmware upgrade procedure.
Was this helpful?
What can we do to improve the information ?