Technical FAQs

Ask a Question

Osisense XS_XS8C2 and XS8C4 cubic proximity sensors SIL2 certified - TUV Nord certificate

Please find attached the TUV Nord certificate for our SIL2 cubic proximity sensors XS8C2/C4*, 4-wires. Please note that the maxi PL or SIL reachable, defined in this certificate, is considering that both sensor outputs are monitored by a safety monitoring unit. This certificate is valid up to July 2017.
Was this helpful?
What can we do to improve the information ?