Technical FAQs

Ask a Question

What is the efficiency of the spur wheel gearbox's and the worm gear gearbox's for the ILE type Lexium Integrated Drives?

Below is the complete listing of all standard versions of spur type and worm-gear gearbox's that are offered with ILE type drives.

Efficiency Spur Wheel Gear:
i=7 : efficiency factor = 0,9
i=18 : efficiency factor = 0,86
i=38 : efficiency factor = 0,86
i=54 : efficiency factor = 0,81
i=115 : efficiency factor = 0,81

Efficiency Worm Gear:
i=24 : efficiency factor = 0,61
i=54 : efficiency factor = 0,62
i=92 : efficiency factor = 0,56
i=115 : efficiency factor = 0,51
Was this helpful?
What can we do to improve the information ?