Technical FAQs

Ask a Question

Osisense XM_XMPC06C2941S701 specifications and how to order in 2015

1) The XMPC06C2941S701 power switch is the "standard" XMPC06C2941 (available under logistic ref. XMPC06C2941AB in 2015, requesting to provide the fluid entries A, B, C, D definition) supplied with S701 specification.

2) S701 specifications meaning
  • 1/2 gas fluid connection drilling in A (see attached file for fluid entries designation)
  • 1/4 gas fluid connection drilling in C
3) How to order the XMPC06C2941S701 reference in 2015 : it has to be ordered under the following logistic reference XMPC06C2941S701AB (internal Schneider rule). Logistic situation : available, in stock in IDC Evreux France.
Was this helpful?
What can we do to improve the information ?