Technical FAQs

Ask a Question

How do I calculate current consumption for Lexium Integrated Drive type ILE2 ?

The actual current consumption is depending on several values, e.g. speed, torque and power losses and is complex to calculate....

However, there is a "simple" calculation procedure which will provide a useable current consumption figure that will meet most needs

P = P_loss + (2*PI*n/60)*Mn
I=P/U

e.g.: P_loss = 40W (typical value), n= 3000rpm, Mn = 0,26Nm ( nominal torque for ILE2x661 taken from product data sheet )
P= 40W + (2*3,14*3000/60)*0,26Nm = 122W
I=122W/24V = 5A

 
Was this helpful?
What can we do to improve the information ?