Technical FAQs

Ask a Question

What is the default IP address of the 140NOC77101?

Title
Quantum 140NOC77101 Default IP Address
 
Issue
Quantum 140NOC77101 Default IP address
 
Product Line
Quantum 140NOC77101
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
 The 140NOC77101 module uses the following default address configurations:

Default IP Address
The default address starts with 10.10 and uses the last two bytes of the MAC address. As an example, a device with the MAC address of 00:00:54:10:8A:05 has a default IP address of
10.10.138.5 (0x8A=138, 0x05=5).

Default Sub-Network Mask
The default Subnet Mask address is 255.0.0.0 (a class A mask).
Was this helpful?
What can we do to improve the information ?