Technical FAQs

Ask a Question

Is there a break down of part numbers for the Magelis Box/Panel PC which explains what each alphanumeric value means?

Issue:
Is there a break down of part numbers for the Magelis Box/Panel PC which explains what each alphanumeric value means?

Product Line:
Magelis, Box PC, Panel PC

Environment:


Cause:


Resolution:
Yes, below is the break down of what each alphanumeric value mean in the part number of the Box/Panel PC.
Was this helpful?
What can we do to improve the information ?