Technical FAQs

Ask a Question

What does FPS/FP/Net means in the Vijeo Design'Air diagnostics?

Issue:
What does FPS/FP/Net means in the Vijeo Design'Air diagnostics?

Product Line:
Vijeo Design'Air

Environment:


Cause:


Resolution:

FPS --> Frames per second (Higher the number the better means more high quality images)
FP --> Frame Processing ---> This is amount of time it takes to process a received frame (Lower the number the better)
NET --> This is the time in between each frame (Lower the number the better)
 
Was this helpful?
What can we do to improve the information ?