Technical FAQs

Ask a Question

Do we have a stepper motor in our product range that complies to the New European IECex standard ?

Issue: Product offer

Product Line: Stepper motor, ExRDM

Environment: Explosion Proof Environment

Cause: Customer need

Resolution: The ExRDM3910 and the ExRDM3913 are our only stepper motors for Ex environment.
Other motors are not in our portfolio and therefore we have no equivalent motor that complies to the IECex standard.
Was this helpful?
What can we do to improve the information ?