Technical FAQs

Ask a Question

Can the Quantum 140NOE77101 ethernet module be assigned an IP address without a CPU module?

No.. A Quantum CPU module must be placed in the rack at minimum to use either a Bootp server to assign a temporary IP address or use the NOE's default IP address to connect to the NOE's web page..
Was this helpful?
What can we do to improve the information ?