Technical FAQs

Ask a Question

Made offline changes and build the Unity Pro project. Once online to the controller, the status is that the project is different and not equal. How do you get the Unity Pro project to be equal?

Issue:
Made offline changes and build the Unity Pro project.  Once online to the controller, the status is that the project is different and not equal.  How do you get the Unity Pro project to be equal?

Product Line:
Unity Pro, M340, M580, Premium, Quantum

Environment:


Cause:


Resolution:
Your options to get the Unity Pro project equal to the controller are as follows:
1 - Download the project to the controller with the new build.
2 - Upload the project from controller.
3 - Unity does an auto save of the last successfully download to the controller.  If this PC was used to download to the CPU previously, then open the projectname.auto.sta project and go online to the controller equal.
Was this helpful?
What can we do to improve the information ?