Technical FAQs

Ask a Question

What is the cable pinouts for the Bus-X (TSXCBYxxxx) cable?

Issue:
What is the cable pinouts for the Bus-X (TSXCBYxxxx) cable?

Product Line:
TSXCBYxxxx

Environment:


Cause:


Resolution:
The pinouts of the TSXCBYxxxx is a straight through cable.
(1 to 1, 2 to 2, 3 to 3 ... 9 to 9)
Was this helpful?
What can we do to improve the information ?