Technical FAQs

Ask a Question

Does Lexium 23 Plus support a relative move when in PR mode?

Lexium 23 Plus in PR mode only supports additive incremental moves.
This means that if you wish to transition from one data set to the next data set the move distance will always be additive.
Therefore, it is not possible to transition from one data set move to another data set with a incremental relative position move.

However, if the moves are absolute moves, then it is possible to transition from one data set absolute move to another data set absolute move and have the motor reach the absolute position of the last data set which was executed.



 
Was this helpful?
What can we do to improve the information ?