Technical FAQs

Ask a Question

Is there an equivalent module to the TM3TI8T with only 4 channels?

Issue:
Is there an equivalent module to the TM3TI8T with only 4 channels?

Product Line:
TM3, thermocouple

Environment:


Cause:


Resolution:
Yes, the part number is TM3TI4 which is an equivalent to the TM3TI8T but only have 4 input channels.
Was this helpful?
What can we do to improve the information ?