Technical FAQs

Ask a Question

What is part number of Connexium switch with Gigabyte SFP interfaces?

Title
Connexium switch with Gigabyte SFP interfaces
 
Issue
Connexium switch with Gigabyte SFP interfaces
 
Product Line
Connexium Managed Switch
 
Environment
N/A

Cause
N/A
 
Resolution
 The part number of a Schneider Electric Connexium switch with Gigabyte SFP interfaces is below:
TCSESM103F2LG0  - 8 x 10/100BASE-TX ports (copper cable), RJ45 shielded connectors; 2 x 1000BASE-fiber SFP fiber ports
Was this helpful?
What can we do to improve the information ?