Technical FAQs

Ask a Question

How do I link my Twido Suite symbols to my Vijeo Designer Project?

To link the Twido Suite PLC symbols to your Vijeo Designer Project, use the following procedure below:

1) In Vijeo Designer, add a Modbus RTU or Modbus TCP/IP driver to the I/O Manager (enable IEC syntax if necessary)
2) Go to the variable menu.
3) Select Link Variables
4) Change the file filter to .xpr
5) Browse to the Twido Suite project file with the extension .xpr
6) Press Open
7) In the Dialog box that appears, select the variables you wish to link and select "ADD".

Was this helpful?
What can we do to improve the information ?