Technical FAQs

Ask a Question

Can I add an expansion rack to an existing Quantum RIO drop using the CCOTF option?

No. It is not possible to add an XBE interface and backplane to an existing Quantum RIO drop using CCOTF.


Was this helpful?
What can we do to improve the information ?