Technical FAQs

Ask a Question

Is there a cable to connect a Quantum RJ45 Modbus Port to a 2-wire RS485?

Title
Quantum RJ45 Modbus Port 2-wire RS485 cable
 
Issue
 Cable to connect a Quantum RJ45 Modbus Port to a 2-wire RS485
 
Product Line
Quantum RJ-45 Modbus port
 
Environment
Unity Pro
 
Cause
N/A
 
Resolution
 The cable part number -  TCSMCN3M3M3S2 - is used to connect a High End Quantum CPU via the RJ45 Modbus port to a 2-wire RS485 network.
Was this helpful?
What can we do to improve the information ?