Technical FAQs

Ask a Question

What are included in the Panel PC maintenance kit part number HMIYPMKT11?

Issue:
What are included in the Panel PC maintenance kit part number HMIYPMKT11?

Product Line:
Panel PC

Environment:


Cause:


Resolution:
The Panel PC maintenance kit consist of the following parts:
  • 1 - 3-way removable connector for 24V DC power supply
  • 1 - 3-way removable connector for 100…240 V AC power supply
  • 2 - protective covers for USB port on front panel (only on Aluminium bezel versions)
  • 10 - replacement filters for fan, including:
    • 5 - for Magelis Panel PC with no PCI slot
    • 5 - for Magelis Panel PC with 2 PCI slots
  • 18 - screw fasteners (Aluminium bezel) or 
  • 14 - fasteners (Stainless steel bezel
Was this helpful?
What can we do to improve the information ?