Technical FAQs

Ask a Question

Why do I get a warning about using a power supply with a 140CRA211xx DIO Adapter?

Title
140CRA211xx DIO Adapter power supply warning
 
Issue
140CRA211xx DIO Adapter power supply warning
 
Product Line
Quantum.
 
Environment
Unity
 
Cause
N/A
 
Resolution
 The purpose of the Warning, is because the 140CRA211xx DIO Adapter has its own built in power supply.
You are cautioned to "DO NOT WIRE THE DIO ADAPTER POWER CONNECTOR WHEN BEING USED THIS WAY"
The two power supplies it can be used with are the 140 CPS 114 00 & 140 CPS 124 00. When the 140CRA211xx DIO Adapter is used with an 8 amp power supply is  will consume approximately 0.5 amps. 
 
Was this helpful?
What can we do to improve the information ?